• AD7150 /AD7156

    We are designing a control handle with proximity detection, meaning, the user must hold or be in close proximity of the control handle to be able to activate it. Functionally I can not seem to see the difference between AD7150 and AD7156, where are the…

  • Difference between AD7745 + AD7156

    AD7745

    AD7156

    The AD7756 states that it is applicable for position detection where as the 7745 is applicable for position sensing.

    As the 7156 includes a 12 bit CDC and the 7745 includes a 24 bit CDC i conclude that this type of wording has been choosen…

  • AD7156

    Hi,

    I am using Eval AD7156 for liquid level measurement application. I would like to add reference capacitance in one channel and level measurement in another channel. Here my doubt is should I connect EXC1 and EXC2 short together??

  • AD7156 x AD7147

    Hello Gentleman,

    We are working with a customer for making one capacitive sensor for detecting finger placement, end application would be for security, eliminating switches for lighting control and access control. It is one innovative product that will…

  • RE: AD7156

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Eval AD7156 integrating with arduino uno

    Here i am trying to comm with I2C through SDA and SCL of Arduino uno board.

    its starting stage im not able to read the data in register of ad7156

    its showing FF for all reg.

    hardware connection in correct and logical level converter connected between…

  • RE: An issue about AD7156

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7156 Eval Board Conversion Error?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 关于AD7156 CDC 电容传感器的疑问

    This question has been closed by the EZ team and is assumed answered.
  • RE: Can I use AD7156 to measure capacitance accurately?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,