• RE: Replacing Tl072CP

    Hi, Dave.

    Yes, both AD712 and AD8512 can be used as VCA. You just have to replace the TL072ACP and you're all set.

    You can purchase the units in the Sample and Buy section of the AD712 product page and AD8512 product page. Just click the links and…

  • FAQ: AD7124-4/8 Standard Silicon versus B-grade

    Question: What are the differences between the standard AD712-4/8 and the B-grade

    Answer: There are some key differences between the B-Grade (AD7124-xBBCPZ/AD7124-xBBCPZ-RL) and the standard (AD7124-xBCPZ/AD7124-xBCPZ-RL) AD7124-4/8. Choice will depend…

  • 关于ad8620线路接法

    本电路图是功率稳定完整描述图,图中绿色标注部分为接口的相关说明,基本原理就是通过光电二极管采集的电压同设定光强电压做对比,最终将输出电压输送给光栅,以此来调节激光器的光强。

    然而涉及到芯片的一些接法实在不知道原理是什么,因为是从其他控制器直接copy过来的板子,所以不知道有些接法不知道是对是错。

    请教大神描述一下一些接法原理:ad8610的接法网络,tl084, ad823,还有ad712的接法,这些都是为了做什么呢?

    电路图附件表示中。其中ad8610部分在最下方。

  • op270做二阶有源低通滤波器,单位增益跟随输出,当输出电压饱和时,输出振荡。

    op270做二阶有源低通滤波器,单位增益跟随输出,当输出电压饱和时,输出振荡。op270纯跟随输出饱和时不会振荡,只有在下图二阶有源滤波跟随输出饱和时振荡,将电容C1拆除后饱和输出无振荡;或者将运放OP270换为AD712饱和输出也没有振荡。请教达人讲解下OP270在这个电路饱和输出时的故障原因和机理,以及AD712没有振荡的原因。谢谢!

  • RE: 请问这个滤波电路设计是否合理?运放工作的状态是怎样的?

    您好,您使用的运放芯片不是ADI的产品。请到相关的技术支持进行咨询。

    另外,如果您需要该芯片的替代芯片,可以考虑AD712,AD8512.

  • AD717X数据采集错误

    关于AD717X使用中出现的状况我描述下:使用7172AD进行数据采集的仪器开机程序运行,测量数据都是准确的,如果这时附近有仪器打开或关闭,便偶尔会影响到AD712的运行,表现的现象就是采集的数据是一个非法的数据,而且一直都是同一个数据,但是控制的单片机是正常的,除了数据采集不正常,其余控制显示都是正常的!我现在处理的方法是程序每运行一次,就对AD7172的寄存器写一次值,便不会出现错误值,即使出现下一个循环也还是正常的,但总觉得不是好的处理方法,也想到AD那么大的一个国际企业,一款产品不可能出现问题而没有发现…

  • ADI院士访谈:如何用先进模拟技术打造完美音效

    ADI Academician Interview: How to Create Perfect Sound with Advanced Analog Technology by ADI_Amy

    This article is the "Electronic Engineering Album" reporter Shao Lefeng interviewed by ADI academician Scott Wurcer (original "using advanced analog technology…

  • RE: ADI院士访谈:如何用先进模拟技术打造完美音效

    文章中相关产品介绍:

    AD524:  精密仪表放大器(http://www.analog.com/zh/specialty-amplifiers/instrumentation-amplifiers/ad524/products/product.html)

    AD524是一款精密单芯片仪表放大器,针对要求在最差工作条件下提供高精度的数据采集应用而设计。高线性度、高共模抑制、低失调电压漂移与低噪声等特性的出色组合,使该器件适合用于许多数据采集系统中。


    产品聚焦

    1. AD524具有保证低失调电压…
  • 极品运放AD827真假的鉴别方法(转)

    现在不良商家造假可谓想尽各种手段,音响市场也不例外,导致假次产品泛滥。下面具体介绍真假运放 AD827的鉴别,希望对广大音响发烧友有所帮助。

       真品 AD827AQ 正反面串号一样,字体均衡呈棕黄色,正面边缘有低于表面模线,12V~18V供电时表层温度达到 60℃,用手按住三秒就会感到非常烫手。如果感到只有一点烫手,表面温度约 40℃,那基本是 OP275 和 AD712的打磨品。AD827AQ全新原装品买 10 片以下价格不可能低于 80 元/片。1~999 片进口价为 8.7 美元,1000…

  • AD7124 input current nonlinearity in buffered mode

    Hello! During testing of the evaluation kit EVAL-AD7124, I've been found that input currents of the buffered analog inputs has strong nonlinear behaviour that depends from the common mode voltage at the buffered analog inputs.

    Test setup was as follows…