AD7091R-5 GPO0 can be set by register as Open-Drain or CMOS, but GPO1 and GPO2 are not explained.
Which one is GPO1 and GPO2? (Open-drain or CMOS)
AD7091R-5 GPO0 can be set by register as Open-Drain or CMOS, but GPO1 and GPO2 are not explained.
Which one is GPO1 and GPO2? (Open-drain or CMOS)
The page 8 of AD7091R-5 datasheet describes VDrive as "The voltage range on this pin is 1.8 V to 5.25 V and may differ from the voltage range at VDD, but must never exceed it by more than 0.3 V", however AD7091R does not have this limitation.…
Hi
I'm a DFAE in Japan. Our customer give us a question. There is a MOSFET inside SDA pin of AD7091R-5. On the other hand, is there NO MOSFET inside SCL pin of AD7091R-5? According to Table 5, we couldn't see Open-drain output about SCL as follows.…
Dear All:
AD7091R-5 table 8. Slave Addresses show AS0 & AS1 pin same time It's can NC ,If ESD conductive test or a lot of noise around the motor ,will it be disturbed by noise or act abnormally? have any suggest to me refer. thnaks
Best
Jac…
Hiroyuki,
The way around this is to leave the power up (if possible) and to write either stop addressing the AD7091R-5/AD7415 to talk or otherwise force those units to go into a low power state. This will prevent the loading with no need for additional…
Hi
Could you please recommend ADI's IC as the device reset for AD7091R-5 ?
Regards,
Hiroyuki
Hi Wollli,
Apologize, I was referring on the wrong device (AD7091R). From the Table 3 of the AD7091R-5, Analog input voltage should be from -0.3V to Vref + 0.3 V only with respect to ground. Having input voltage greater than the maximum voltage will…