• The figure shown on order information page of AD706 data sheet was WRONG. The SOIC shows DIP outline and the DIP shows the SOIC outline.

    The figure shown on order information page of AD706 data sheet was WRONG. The SOIC shows DIP outline and the DIP shows the SOIC outline.

  • 放大器压摆率和应用领域

    请帮忙解释一下为什么音频电路里面运放的压摆率都达到甚至超过10V/us  比如NE5532 9V/us AD827 35V/us TL084 18V/us 

    而用于传感器,电压,电流,温度等小信号电路里的运放 都很贵但是压摆率通常都在1V/us 以下  AD706  ,OP07 ,OP27  甚至能低到0.2V/US 

    为什么在工控测量领域的运放可以选用这么低压摆率的?而音频电路里却动辄十几V的压摆率?什么情况下需要注意运放的压摆率呢

  • RE: ADXRS620 Noise Density和电源供电的问题请教

    您好,我现在选择的AD是AD7606。

    您说的把VRATIO和ADC一起供电,指的是把VRATIO和ADC的Vref一起供电,对吧?可惜的是AD706的Vref只有2.5V,而VRATIO要5V,这种情况下有什么好的解决方案没?

    另外,ADXR652的AVCC怎么处理呢?我的想法是把AVCC、VDD连在一块,然后和AD7606的AVCC连在一块,最后通过一片LDO供电。不知道这样是否合适?

    ADXR652的AVCC最大需要多大的电流?手册上只说了一个总电流,不知道这个总电流是指VDD还是AVCC…

  • 资源转发---仪表放大器设计指南

    仪表放大器设计指南

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…