Hi
I'm a DFAE in Japan. Our customer is looking for ADS7-V2EBZ reference design like this. He wants to evaluate AD6674. Could you help this?
Regards,
Hiroyuki
Hi
I'm a DFAE in Japan. Our customer is looking for ADS7-V2EBZ reference design like this. He wants to evaluate AD6674. Could you help this?
Regards,
Hiroyuki
I'm designing an ADC circuit with 0-100Mhz single end input. suppose to use ADL5569 as input amplifier, which also convert the single end input to differential. as the DC signal have to be sampled, so the whole circuit is DC coupled.
The AD6674 require…
您好,我是一个在校学生,目前有个项目,需要用AD6674设计一个高速采集卡。我在贵公司的网站上没有找到AD6674评估板的原理图和仿真文件,请问我如何才能获得AD6674评估板的原理图?谢谢了!
您好,我是一个在校学生,目前有个项目,需要用到AD6674做数据采集。我在贵公司的网站上没有找到AD6674评估板的原理图和仿真文件,请问我如何才能获得AD6674评估板的原理图?谢谢了!
Hello,
I am looking for Dual channel ADC eval board with 14 bit wide and sampling @ 1 GSPS.
Analog bandwidth is fine up-to 500 MHz.
Where I got several options
1) AD6674-LF1000EBZ vs AD9234-LF1000EBZ / AD9680-LF1000EBZ
For RF spectral data recording…
在公司看了一下AD6674的手册,其中有一个VDR的功能,是做DPD的时候用的,但是不明白为什么这种功能的好处是什么? 降低了有效位数,减小了动态范围,是为了换取更大的带宽吗? Thank you!
另外在官网上还没有上传AD6674的手册,可以麻烦发送一份吗?
Hello Nils,
The differences between AD9234 and AD9680 are highlighted at: Compare AD6674-LF 1000EBz vs AD9680-LF1000EBZ / AD9234-LF 1000EBZ
Throughput needed by the ADC would be sampling rate x sample size (1gsps x 2bytes= 2GBps). ZC706 HP ports are…
上海,浦东新区碧波路889号,从事基站RRU开发和架构设计,关注ADI高速产品例如时钟:AD9549、AD9523、ADC:AD6657、AD6674、DAC:AD9142、AD9154、AD9144、PLL:ADF4351、解调器:ADRF6820、OP:ADL5566、AD8376、调制器:ADL5375、ADL5371、ADL5372等等。
系统方案 APM
技术指南 Mini Tutorial
技术文章 Tech Article