• AD667: supply voltage

    Q1. Does it matter if the supply rails do not rise in voltage together
    at power-up?
    Q2. Similarly does it matter if the supply rails do not fall in voltage
    together at power-down?
    Q3. Will the AD667 tolerate one or more of the supply rails stuck…

  • ad667: If CS\=0 are input latches transparent

    For AD667 If cs pin is grounded . Does DAC continuously convert the changes in
    the input to Analog out..

     

    Pages 6 and 7 of the AD667 datasheet explain that the CS\ and Ax\ signals are
    LEVEL TRIGGERED. The Truth table II on page 7 shows that when…

  • RE: First output voltage of AD667

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Can I connect inputs on AD667 directly to digital outputs on Atmel SAM3X8E ARM Cortex-M3 CPU?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: I'am having a trouble connecting the AD 667 to a pic microcontroller, do i connect all the inputs to the pic or the cs and A3-A0 pins only ?

    Hi,

    Just to clarify, do you intend to display the 16-bit counter/timer into analog form using AD667? If yes, then since AD667 is using a parallel interface, you should convert the 16-bit register into a parallel form so that each GPIO pin will handle…

  • DAC type?

    Hi all, i am a new to this forum but i have a question and i hope someone can help me. I am a student and i am building some equipment for an AFM and i am using a DAC AD667. My question is what type of DAC that is (pulse-width modulator or Oversampling…

  • AD6676EBZ system configuration

    Hello,

    I am working on ZC706 with AD6676-EBZ, ref design Vivado 2014.4.1. I am trying to capture the data from DDR3 using adc_capture function given in noOS driver (ad6676_ebz.c). I'm using these two functions:

    adc_capture(16384, ADC_DDR_BASEADDR…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…