• AD6650: Footprint

    On the component, you have a pad where is attached the solder ball. This pad
    size is very important because it is the size that we must apply on our PCB to
    get a correcot solder joint. It had be shown that if the footprint on the PCB
    is larger…

  • AD6650: Antialiasing filter

    In  datasheet to IC AD6650 in SPECIFICATIONS following parameter
    is pointed:
         
                                             min.  nom.  max.
          ________________________________________________________
          BASEBAND FILTERS
          Bandwidth         Full        IV   3.36  3.5  3.64  MHz

         
    Could you explain this? What narrow…

  • RE: AD6630 to AD6650 interface problem

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADRF6650 PLL doesn't lock on evaluation board

    Hello,

    I'm using ADRF6650-EVALZ board and ACE software but I did not succeed to get DS1 on or LOCK_DETECT register set to 1 meaning PLL is locked. 

    My RF reference signal is a sinus at 15.36MHz and 2.5Vpp in order to obtain 30.73MHz thanks the input…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…