FAQ
In case of chip utilization of AD6636 there was the following problem:
at a zero spectral bin there is always a parasitic spectral component of which existence it is possible to get rid changing values of the register CIC scale factor. But at the same…
通过FPGA进行并口的时序控制,寄存器已经成功读写,官方文档上BIST相关寄存器 BIST Control设置使能,并将计时器赋值,输入和通道寄存器也设置,直接读取BIST I/Q Path Signature Register后的值还是默认值6636,不是应该产生一个随机数吗?有哪位大神指点一下想使用这个模块该怎样设置寄存器啊?
Hi,
The legacy AD6636 was released some 13yrs ago and has been on the "not recommended for new designs list" for many years. Due to this ADI support is primarily limited to continuing to source the legacy AD6636 components for existing legacy customer…
Hi Dave,
When the AD6636 was initially released it may have had an edge over an FPGA in terms of power/function, but FPGAs are continually evolving to smaller process geometries which leads to lower power. So I expect today's FPGAs would likely come…
I am working with the AD6636 (DDC) and AD9251 (ADC) , both of which have a PN sequence generator, usually used for BIST purposes.
I am interested in vaildating my raw data streams from these devices when they are outputting the PN streams,
Can anyone…