• RE: looking for the AD648 SPICE model

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Help with AD648 Opamp when very low input signal change

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Help with AD648 Opamp with very low input signal change

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Need AD648 spice model. Thank you. fausto Bartra

    Does anyone has the spice model for the AD648 OP-AMP (or similar)

    Thank you

    Fausto Bartra

  • RE: Effect of OP amp change

    Hi Kanzawa san, 

    Great find, I was about to recommend using this tool. Looks like the AD826's input bias current is quite large resulting in a huge increase in ppm error. I suggest looking for other amps. The AD648 looks like a good choice. 

    Regards…

  • RE: AD648AH obsolete date and suggested replacement part?

    Hello Hunter, 

    The AD648AH is no longer available. We only offer the AD648 in grades J and K. The J grade should have the same performance as the A grade but has an operating temperature range of 0 to 70degC. 

    May I request again for what you are looking…

  • 最爱ADI放大器之AD215

    最爱ADI放大器之AD215 by 1901818846@qq.com

    AD215是一款速度高达 120kHz的高速隔离放大器,其在强干扰的工业环境下的应用非常广泛,比如电机控制和多路高速数据采集系统

    1. AD215的内部结构与工作原理

    AD215是美国AD公司出品的模拟信号输入输出隔离放大器,是技术先进,功能完整的隔离放大,大多数的模拟信号经 AD215隔离后的动态性能
    和频带宽度均不受影响AD215的速度和准确度可满足几乎所有的测量场合的速度和频带的应用要,它的额定功率带宽为120k…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…
  • 最爱ADI放大器之AD215

    AD215是一款速度高达 120kHz的高速隔离放大器,其在强干扰的工业环境下的应用非常广泛,比如电机控制和多路高速数据采集系统

    1. AD215的内部结构与工作原理

    AD215是美国AD公司出品的模拟信号输入输出隔离放大器,是技术先进,功能完整的隔离放大,大多数的模拟信号经 AD215隔离后的动态性能
    和频带宽度均不受影响AD215的速度和准确度可满足几乎所有的测量场合的速度和频带的应用要,它的额定功率带宽为120kHz,满量程线性误差0.005%,隔离电压有效值为1500V,适用…

  • 10/12/16 Challenges for Electronic Circuits in Space Applications

    This webcast provides insight into the challenges engineers encounter in implementing circuits for space applications. Concerns about reliability, radiation effects and the ability to tolerate harsh environmental conditions requires special attention…