FAQ
Hi
I am FAE in Japanese distributor.
Our customer produces his product using AD633.
He is calibrating AD633 at Vs+=15V, Vs-=-15V, X1=0V, X2=0V, Y1=2.5V, Y2=0V.
After the calibration, he test AD633 the condition is followings.
Vs+=15V, Vs-=-15V, X1=0.2Vsinusoid…
Hi all, I wanted to use either dy/dx or the double angle formula to add overtones to an audio signal ( specifically with advancing the slew rate in a manner proportional to frequency, not limited by an RC constant). The AD633 looks great, and even will…
Hello,
I need some help with my circuit. 2 sine waves are generated with 2 AD9833's, then are amplifier and filtered with 2 1st order low pass filters, and then connected to the AD633. As the sine wave have about 200 mV offset, I'm using 2 coupling capacitors…