• AD630 help

    hi everyone

    I’m looking to implement an amplifier in the range of 100KHz to 2MHz to obtain amplitude and phase information.

    Whether the AD630 will be ok for this frequency range or is there another device out there that is better?

    If the AD630 is…

  • AD630 help

    Hi All,

    I am designing a light scattering sensor then needs ambient light rejection.

    I have a 500Hz PWM modulated LED source that shines into a sample volume.

    A collimated photodiode picks up the scattered modulated light, as well as higher frequency…

  • ad630

    hello,supporter!

    What is the meaning of the inverting terminal -V in the integrator?

    How is the feedback resistor of amp connected to the output of the integrator?

    thank you!

  • AD630

    Hi,

    I designed a precision phase detector using the AD630.The measurements signals (sine wave) in the range of 10kHz -500kHz with maximum Vp= 5.0V. The device is versatile and within my budget. For this purpose I follow the design in circuits diagram…

  • ad630

    AD630里面有乘法器吗?他是如何调制信号的,积分器是用来干嘛的?哪个征文看不懂谢谢

  • AD630

    你好,adi工程师

    这里的-v有什么用?

    RF是在怎么对AMPa 进行反馈的,rf为什么不在amp a输出端而在积分器的的输出端?

  • AD630 alternative

    I've been using the AD630 to demodulate a 1kHz sensor output.  It works very well, but is prohibitively large for embedded applications.  Is there a smaller alternative to the AD630 for demodulation / synchronous detection?  Is it possible to use the…

  • AD630 debug problem

    hi

    I’m looking to implement an amplifier in the range of 100KHz to 2MHz to obtain amplitude and phase information.

    I followed the design in circuit diagram 9a Gain-of-One balanced modulator. Pin 3-6 and the capacitors with powers are not connected.

  • AD630 balanced modulator

    I am using AD630 as a modulator. The carrier input is a sinusoidal signal from 37mV to 645mV with a frequency of 10kHz; the modulation input is a sinusoidal signal from -1V to 1V with a frequency of 1kHz. A 100μF DC blocking capacitor is used at the carrier…

  • AD630 Supply Voltage

    Hello there,

    I'm relative new in designing analog circuits and in understanding IC specs, so this questions seems a little easy to answer for an expert I think.

    The data sheet of the AD630 (http://www.analog.com/media/en/technical-documentation…