• AD625关于失调失调电压关于相对于时间的比值指标

    AD625失调电压相对于时间的比值指标,这个参数在datasheet里没有给出来

  • AD621: PSRR

    Q

    We have an AD621 measuring the voltage drop across a 2.5R sense resistor.
    We are measuring 78uV of noise at the output of the AD621 with x10 gain. I have
    taken the inputs 2,3 out of circuit and directly shorted them. The noise is
    still there.
    The data…

  • RE: AOP Instrumentation

    Hi ,

    Yes, the input noise voltage AND the "0.1Hz to 10Hz" Vnoise (Vpp) are good parameters to choose for when trying to find a part that can extend the lower detection voltage range to 1uV, as in your case.

    For example, you can use this…

  • 信号放大高增益精度

    运放用的AD625,增益精度能达到0.02%,外围可编程的放大电路,怎么能达到0.05%的精度啊?算了几天都不行,电阻目前选用的是0.1%的精度。有什么办法能提高电路的精度呢?

  • RE: ADC-FMCADC2 clocking

    Hi,
    1. You can find on the ADI wiki page AD-FMCADC2-EBZ FMC Board [Analog Devices Wiki]:

    Alternatively, the oscillator can be disconnected and an external clock source connected by only changing two components on the board.

    Yes you are right, de-solder…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…