FAQ
hi,
Thanks for your answer.
my operating frequency is really at 500KHz ( and I already test until 1MHz) I noticed that the cut off is around 700KHz (-3dB). I don't understand why working at 500KHz is not recommanded for AD623.
if you have another…
Hi YuxiangRousi,
Good day!
Apologies we missed this email thread, in case you haven't figured out the issue with your circuit, we're here to help out.
For this question, will it be okay to share the circuit diagram you used? We may be able to spot…
I am using an AD623 with a MC33161 voltage monitor to monitor the temperature of a part.
V_SET is around 1.1 V, V_ACT the current temperature monitor voltage being equal to V_SET when the temperature is reached.
Reference voltage for the AD623 is 2.54V…
I have a board that uses an AD623. See attached schematic
The input voltage is 1.45V, the amplifier gain is 5.65, the output voltage is (1.45-0.97) * 5.65 = ~2.7V. Supply voltage is 5V
The problem I see is that with devices with date code 2022 (Other…
This is an old thread, and perhaps nobody is looking at it any more. But Gustavo's answer doesn't quite make sense to me -- in all ECG applications that I know of, you measure the voltage *difference* between two electrodes. In that case, why wouldn't…