• what other component is similar to AD607 / AD61009?

    currently i am using orCAD but there is no library for this component. anyone can help me?

  • Using an AD607 for BPSK demodulation.

    An answer to an older question on the AD607, https://ez.analog.com/rf/f/q-a/75353/ad607-for-bpsk-detector-on-lf-30-120khz, mentions an attached paper on using the AD607 for BPSK demodulation, but the paper is no longer attached. Which paper is it? Is…

  • AD607 with Costas loop

    Hi 

    I would like to use AD607 to demodulate BPSK/QPSK signal, and I would like use the quadrature VCO on AD607 to construct a Costas loop to recover the carrier.  My thought was first feed in a 10.7MHz to FDIN, demodulated I Q will be multiplied in DSP (digital…

  • RE: AD607

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD607

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD607

    Hello,

    is it possible to feed FDIN input of AD607 quadrature section

    with a square wave signal ?

  • AD607(2)

    Thanks for answer, square wave in FDIN work OK

    Other two questions:

    1) how much is the maximum rating of LO power
    (in the IQ section)?


    2) is it possible a use (atipical) of AD607 IQ section
    as a IQ upconverter (audio baseband in input), up to
    12 Mhz…

  • RE: AD607 for BPSK detector on LF. (30-120kHz).

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD607的混频器

    AD607的混频器能否用于AM信号上混频。

  • AD607输入频率限制

    AD607 RF输入频率可以多低,可以为190KHZ-2MHZ吗。