• AD603的一些资料

    论文:增益可变运放AD603的原理及应用

    论文:基于AD603的时变增益放大器的实现

    论文:AD603在信号采集系统中的应用

    论文:AD603及其在AGC电路中的应用

    最近在做程控滤波器搜集了一些AD603的资料,和大家共享!

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    南京,江宁,医疗电子,关注AD9218,AD603,AD8001,AD8138

  • RE: Evaluation board size of AD603

    Hi Akira,

    Please see image below for the AD603 board dimension (in inches).

    Regards,

    Phil

  • RE: DC coupled VGA with single-ended in/out?

    Jose,

    One other suggestion. Look at the AD603, older part, single ended, SOIC package.

    Best of luck,

    Steve

  • AD603 outpout impedance match

    Hi all,

     

    I am using the evaluation board of AD603 to control the output power of a VCO. The problem is  the input and output impedance of this VGA is not 50 ohm. But all of my other components have a 50ohm impedance. 

     

    For the input port, I put a 100ohm…

  • thermal spec of AD603

    Dear ADI support Team,

    I need AD603's Tcase spec, but I didn't find it in datasheet.

    Can you please kind help to provide it? Thanks!

    Henry

  • AD603问题

    AD603由+5v和-5v供电,信号输入为零但是芯片发烫输出超过3V为何?有人遇到过这种问题吗?原理图如下