FAQ
We need to know if the AD600/AD600j PSPICE Macro has Noise modeling.
If it does, where is it specified at their .CIR file?
If it doesnt, how can we edit it with their datasheet specs?
Thank you for your support!
Hello,
I, Satyabrata Sarangi, am using AD 600 in a cascading mode to get 80 dB gain. The problem i am facing is always i am getting an amplified output, with a larger bandwidth. If the original signal is of 1 MHz, i am getting a 25-30 MHz signal as output…
Q.
What is a VGA
--------------------------------------------------------------------------
A.
The TLA VGA stands for variable gain amplifier. Dr. Barrie Gilbert, a EEEE fellow, ADI fellow and world reknowned expert invented the VGA with AD600 and AD602…
i am using LDO from analog devices ADM7150 to generate the output of 5 V from an input supply of 12V. Enable pin is parmanently connected to 6V by using a divider circuit at input supply. I am using this circuit exactly in same manner as given in data…
I want to cascade 3 RF gain stages using ADL5611. I power each ADL5611 directly from a laboratory power supply of 5V. Individually each IC draws a current of 85-90mA. But when I power up two of them together the current reaches 400 mA(170mA expected)…
I'm trying to use the AD600 (as well as some other components, but the AD600 for now) in a a high speed application, but do not have circuit boards yet. The part does not have an evaluation board, but I'm not sure if I can use the white/breadboard…