• AD597: Gain adjustment

    Please can you assist with the following.  With regards to the gain, is there
    some setting/gain resistor which has to be included? If so between which
    terminals?

     

    No.
    It  is not possible to lower the gain of the AD597 by connecting a potential…

  • AD597 output saturation by open thermocouple

    Hello,

    AD596 and AD597AH (H package) has the alarm function for detecting an open thermocouple. There's following description in the datasheet.
    "If the thermocouple loop becomes open, one or both of the inputs to the device will be deprived of bias…

  • Max Temperature measured by AD597:  Type K Thermocouple Conditioner

    Hi,

    In AD597 datasheet (Type K Thermocouple Conditioner) the temperature range is -200°C...+1250°C.

    And +1250°C measurement is achievable under +15V power supply.

    I'm interested in increasing upper limit up to +1500°C

    Would stay the limit +1250…

  • AD595: Accurate signal conditioner

    I have compared the AD595 and the AD597, and the AD597 seems to have a better
    precision (+-1°C) than the AD597 (+-4°C). Can you tell me why? Economical
    reason? Technological reason?
    Do you have any solution to get a better…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • Reading thermocouple correctly with a 2 ground connections.

    I have a Cylinder head thermocouple which is electrically connect to the head. The electronic circuit that is attached to the AD597 output, has the same ground -ve. I therefore have a ground loop. Any suggestions as to how get the AD597 to read correctly…

  • RE: AD597AHZ got burnt

    Hello ahov90,

    You can try double checking all of your connections and verifying that the AD597 is being powered when you expect it to.  Can you attach a schematic of your system as well as any photos of the waveforms you are seeing?  I may be able to help…

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    南京,御道街,做信号采集及处理,关注AD597和AD584.

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…