Hey,
in the "Preliminary Technical Data" of the Evaluation Board of AD5933 there is the "EVALUATION BOARD SOURCE CODE EXTRACT".
link:
Hey,
in the "Preliminary Technical Data" of the Evaluation Board of AD5933 there is the "EVALUATION BOARD SOURCE CODE EXTRACT".
link:
Hello,
AD5933 has real data and imaginary data register (consisting of 2 8 bit register). they store data in 2's complement form(as per datasheet).So does they store 2's complement byte wise? or first they calculate 2's complement of all 16 bit data…
Hi ,
I want a simple reference design for ad5933 4-write isolation bio impedance project .
Thanks.
Hello,
I am using the AD5933 Eval Board to measure a charateristic phase shift of an impedance sensor. Between 5 and 100 kHz I get decent values with MCLK setting to 16 MHz.. For measuring at lower frequencies (1-5 kHz) I set MCLK to 2 MHz but now my…
Hi,
AD5933 supposed to be able to measure the battery cell impedance as stated in its datasheet first page in application section. My question is: the battery cell usually has a range of mili ohms impedance which is out of the AD5933 range. Is there…
Does AD5933 Rev.C evaluation board & Tools can measurement the frequency sweep 1HZ ~ 100KHZ from the RFB & Z(R or C) value?
Dear all,
Could you please discuss why the AD5933 has been provided with the impedance measurement method it holds. There must be some advantages refereeing to it, only that I don't really figure them out. I'm interested in finding out the theory behind…
Hey,
I am trying to Write/Read to/from AD5933 Chip (Impedance Analyzer) from Matlab using I2C PROTOCOL.
For beginning I checked if the communication between the computer to the chip is working:
and then I ran it:
why I get an error?
Do I need to write…