• AD592 connecting capacitor

    Hi,
    Is it possible to connect large capacitor between PIN1 and PIN3 of AD592?
    Does it affect accuracy or dc performance?
    If it affects them, I'd like to know to what it affects and up to how capacitance value recommended.
    Our customer would like to…

  • AD592 temperature transmitter

    Dear All

    Could you explain in easy words how to build a 4~20 mA current loop transmitter using the AD592 current output precision IC temperature transducer? The desided range is from 0 to 50C and it will be connected to an Yokogawa paperless recorder…

  • The resistance of pin(+)-Pin(-) AD592

    Dear Sir/Madam,


    Our customer found the bad resistance AD592 of between pin(+) to pin(-) in their acceptance inspection.

    The way of inspection is to use DMM.

    1; The stick ( + ) of DMM put on your pin( +).

    2; The stick ( -) of DMM put on your pin…

  • AD592 output is incorrect.  What am I doing wrong?

    I am using an AD592 in a circuit powered from 5V (of a USB port).  the 5V is connected to AD592 pin 1, then pin 3 of the AD592 to a 10k, 0.05% resistor to ground.

    When I measure the resulting voltage I am getting 2.630V and I confirmed using a Fluke 287…

  • Can I obtain the AD592C's die pads xy coordinates for wire bonding in an LTCC module?

    Can I obtain the AD592C’s die pads xy coordinates for wire bonding in an LTCC
    module?

     

    The AD592 die pads coordinates are :


    V+
    X= 593um, Y= 105um

    V-
    X= 593um, Y= -318um
  • RE: Tranducer P/N AD592ANZ

    Hi,

    What we recommend requires power. Supply 5V to the + pin, place 1k resister at the - pin going to ground and measure the voltage across the resister, as in Figure 4 of the AD592 datasheet, and check if the output tracks.

    Regards,

    Karen

  • RE: Is this driver compatible with AD592CN sensor?

    Hello, chris_analog.

    Maybe you don't need my answer one month ago, but anyway.

    Of course you can use Temperature Controller with AD590 or AD592 sensor type. These sensors are the same and have very slight differences. Temperature Controller will…

  • RE: AD592AN total error

    Hi Anuj,

    Apologies on my late reply here. AD592 is quite an old datasheet, and it seems this plots at not very well documented. However, they might be showing the performance across temperature across 4 devices. The second plot, in turn, helps understand…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • RE: 听ADI资深同事分享会后整理——常见的几块ADI传感器及信号调理电路

    温度传感器

    温度是到目前为止被检测最多的物理变量,因此其检测方式之多也就不足为奇。最常见的是热电偶,其温度检测范围非常宽,而且相当容易构建。热电偶精度高,使用时间长。

    RTD或电阻温度器件更容易使用,安装简单,具有良好的温度范围和线性度。热敏电阻可以做得极其小,因此灵敏度非常高。它是一种指数型器件,线性度很差,但对许多应用而言是相当不错的。我们还会讨论半导体器件,它具有标准半导体的温度范围,相当精确,而且很容易用在硅电路中。

    墙裂推荐几款主流的模拟温度传感器,电流输出传感器…