• 4-20mA电流源

    ADI专家好!

        有一个项目的需求是:

        1. 产生4-20mA的电流源,精度0.1mA;

        2. 板卡只有15V电源输入和电流输出两个端口;

        3. 板卡的电源由远端的设备15V电源提供,板卡的电流输出在远端设备里通过一个小电阻接到15V电源对应的GND上,也就是说板卡这里没有地;

        我之前打算用AD586电压基准源和精密可调电阻实现,但发现电流最大只能到10mA,而且由于芯片本身的Ibias导致电流有一些偏差,AD587的Ibias好像更大,请问ADI公司的产品有没有可以实现类似功能的芯片或方案…

  • AD7176-2采集直流电压,数据曲线呈现锯齿波?

    您好,我使用ad7176-2遇到问题,

    使用AD7176-2采集直流电压信号,该直流信号是ad586产生的5V信号,电路图照估板电路设计。信号首先经过ad8475芯片衰减(0.8倍),再进入ad7176-2。采样率分别设置5次/秒,24位数据。对数据测试画图发现呈现锯齿状,测试数据和曲线和电路图见附件所示,最大值=5.0321V,最小值=5.0311V,和datasheet差别很大。

    我后来又用1.6V碱性南孚电池测试,数据也类似。是我哪个寄存器没设置好吗?

    此外我想测量3mv-100mv的直流信号…

  • RE: what is wrong with my program? AD7780 simple issue

    Dear Sir thanx alot for your reply

    My supply voltage and reference both are from the same node of a filtered output of the part (AD586) which is a precised out put voltage part of 5 volts

    and the input are shorted togeather to gaurantee a 0 volts…