• Successor to AD586

    Hi

    Could you please recommend the successor to AD586?

    Regards,

    Hiroyuki

  • AD586 Trimming

    The AD586 (5V reference) has a trim pin on it.  I would like to use that trim pin to crank the reference output up to 5.12V.  Unfortunately, there is no equation to help me select the proper resistors needed to do this.  Figure1 of the datasheet shows resistors…

  • ADXRS620 VRATIO和AVCC供电问题请教

    问题一:我用ADP7102ACPZ-5.0-R7给VDD和AVCC供电5V,用AD586给VRATIO单独供电5V,但是ADXRS620的数据手册中说VRATIO绝对不能高于AVCC,这样就让我很头疼,因为ADP7102ACPZ-5.0-R7生成的5V跟AD586生成的5V都是有误差的,这样就不能100%保证VRATIO不高于AVCC;请问VRATIO是绝对不能高于AVCC还是能稍微高于AVCC?

    问题二:为了绝对保证VRATIO<=AVCC,我考虑用AD586给VRATIO和AVCC供电,但是我的系统里有3个ADXRS620…

  • AD586BRZ. Marking code.

    Hello! Can you tell me, please, the information about the marking code on the AD586BRZ voltage reference?

    Which symbols should be on the package and what does they mean?

    I haven't found this info on the AD's datasheet (www.analog.com/.../AD586…

  • RE: 请问AD586的问题

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD586LRZ input voltage range

    Hi Tony,

    I still need to verify the input voltage range of this part to the product owner. Meanwhile, what drives you to use this reference voltage? This part is kinda old (20 years ago). One of our expert recommend the ADR435 for 5 V reference voltage…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • RE: ICP Piezo Force Sensor Interface to microcontroller

    Greg,

    I am considering mid-reference to be the middle of the ADC's reference. In other words, if you supply your ADC with 5V reference, then it would be 2.5V. You will want to drive the reference pin this way because your signal will be bipolar, and…