• AD584 output trimming

    Hello,

    I need to trim AD584 in order to have a 5.12V voltage output. In the datasheet there isn't a formula to calculate the resistive voltage divider for output trimming.

    Can someone provide me the formula, please?

    Best regards,

    Lorenzo

  • AD584: output pin

    Hello,

    I have a question about output pin (1 pin) of AD584.

    Please teach me the maximum value of the capacitor that can be connected with this pin.

    Best Regards,

    Mr.K

  • AD584 dropout voltage measurement

    Here we got a question of AD584 from one customer.
    He would like to know the minimum input voltage for 5V output.
    I did not find this spec in the datasheet.

     

    In general, all references have a certain amount of dropout voltage that…
  • AD584是否可输出1.2V

    可否把AD58416脚短接,形成参考源跟随的方式,输出1.2V,若这样做输出电压的稳定性如何?

  • AD584是否可输出1.2V

    可否把AD584的1和6脚短接,形成参考源跟随的方式,输出1.2V,若这样做输出电压的稳定性如何?

  • MIL-STD-883 compliant version of AD584

    hello,

    Dose the suffix "B" of AD584TH/883B mean compliant with MIL-STD-883B?

    if yes, is there a plan to get compliant with the latest version ( MIL-STD-883K)?

    Best regard,

    Yuki.

  • RE: Can i use +7v supply for AD8561 to generate +5v output with 8ma load?

    Hi Arpit,

    Can you clarify whether your question is on the AD8561 (as in the title) or AD584?

    With regard to the AD584, based on the datasheet, yes, you do need 2.5V headroom from output to supply.

    Thanks!

    Kris

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    南京,御道街,做信号采集及处理,关注AD597和AD584.

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • DC Voltage Calibration Sources for the ADALM1000

    Just how good are the voltage measurements you make using USB based instruments such as the ADALM1000 or Analog Discovery? How would you find out? You could always check the readings against a bench DMM but a good DMM can cost hundreds of dollars. Instrument…