• RE: AD5790 initialization using SPI commands

    Hi morphy89,

    SPI and I2C protocols have a distinct implementation. You can easily distinguish it by the number of digital lines used. SPI uses 3 or 4 wires while I2C only has 2 wires.

    You may want to refer to the following links for the SPI & I2C protocols…

  • Interface AD5790 evaluation board and RPi 3

    Hello.

    I would like to write my driver for control the AD5790 DAC with Raspberry Pi 3 (RPi).

    I have an evaluation board (eval board) AD5790. The schematic is (see the photo below):

    voltage from external power supply:

    VDD = +11.67 V, AGND = to analog…

  • RE: What's the temperature drift of the output of EVAL-AD5790 ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5790的ADI评估板EVAL-AD5790的输出的温度漂移是多少?

    AD5790的ADI评估板EVAL-AD5790的输出的温度漂移是多少?


    是否有类似这种超高精度(20位),但是温漂要很小的评估板?

  • Controlling an AD5790 using RPi3 & linux iio driver

    Hi-

      I am trying to control an AD5790 DAC with a Raspberry Pi 3 using the linux ad5791 driver to control the DAC through it's SPI interface.  The Raspberry Pi is connected to the DAC through an EVAL-AD5760_80_90SDZ board.  To do this, I've been following…

  • AD5790 Block diagram of the LabView program

    Hi,

          I am currently evaluating AD5790:System Ready 20-Bit, ±2 LSB INL, Voltage Output DAC and I would like to have an in-depth understanding of how the SDP and the DAC , AD5790, communicates so I would ask if I could have a copy of the block diagram…

  • binary compatibility between AD5790 and AD5791

    Hello,

    I wonder whether the AD5790 and the AD5791 are compatible regarding digital interfacing and programming.

    Are there significant difference besides package and the integrated reference buffers of the AD5790?

    Best Regards,

    Norman Werner

  • RE: What the difference: AD5780, AD5781

    Hi byliu,

    The AD5781/AD5791 offer better accuracy (INL and DNL for example) compared to AD5780/AD5790. 

  • RE: AD5781 Vout update after RESET

    Hi Mark

    Thank you very much for you support !

    I would wait for 100uSec, considering a variation and temperature changing.

    Even AD5780,AD5781,AD5790,AD5791,AD5760,AD5762R,needs this waiting time, right?

    Regards

    moto

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    天津,光荣道,我做印刷设备,我关注AD5790在信号调理中的应用