• AD8145 doesn't work exactly.

    Dear Sir/Madam,

    I need your help.

    My schematic:

    cf5b8619e13a6629748eb9fcb37b1341.bin

    VREF is provided directly by AD5765. I set the common mode voltage of Vin to 0.5 V and the differential mode voltage to 1.0 V.

    AD5765's output voltage is set to…

  • AD8145使用问题

    电路图如下:


    其中Vref 由ADI的DAC芯片AD5765输出端直接提供,VIN施加共模为0.5 V,差模为1.0V的差分信号

    预设AD5765输出电压为0 V.

    实验中,我测试芯片AD8145的REF引脚,发现该电压并不是AD5765预设的电压值(当然此时,AD5765输出电压跟REF端几乎相等,显然不正常)REF端输出一个与VIN同频的信号,且其峰峰值随VIN的频率变化如下:

    及其对数坐标表示:

    我的问题是:

    REF端之所以不跟随AD5765,是因为AD5765的驱动能力不足造成的吗…

  • AD7699: Sharing SPI bus

    Hi, I have a couple of question about using an AD7699;

    Some background: Basically I'm developing a product where we need to sample two channels of the AD7699 at very specific time intervals (around 40uS), so I'll be using an timer interrupt to control…

  • DAC datasheet里面的“Short Circuit Current”和“Load Current”有什么区别?

    这是AD5765DATASHEET里面关于输出电流的说明

    Short-Circuit Current   10   mA typ     RISCC = 6 kΩ; see Figure 23

    Load Current              ±1   mA max    For specified performance

    我的理解:

    Short-Circiut Current  规定DAC的最大输出电流,

    那这个Load Current 规定什么?是DAC接上负载后,流经负载的最大电流吗?

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…