FAQ
Hello,
We are using AD5764 DAC, which is on spi interface
added the following dac device tree
vdac: fixedregulator0 {
compatible = "regulator-fixed";
regulator-name = "vdac";
regulator-min-microvolt = <5000000>;
regulator…
Hello,
we are using AD5764, we have enabled AD5764 driver in linux driver configuration.
we are able to write to out_voltage0_raw, out_voltage0_calibscale, out_voltage0_calibbias files.
When tried to read out_voltage0_scale, following error was observed…
Hello ALL,
I'm using AD5764,
followed https://wiki.analog.com/resources/tools-software/linux-drivers/iio-dac/ad5764 to enable the driver.
I'm able to see the dac device after changing the device tree. Here is the log attached.
root@fps_clc:/sys…
Hello,
My customer asks some questions about using ISCC pin of AD5764.
They say that ISCC pin seems to control a Short-Circut Current which controls a quantity of current to Vout pin at short status of circuit.
So please check below questions and let…
Hello - I have p/n EVAL-AD5764REBZ which is a 4 channel DAC. I would like to know the basic steps to build the driver located at: https://wiki.analog.com/resources/tools-software/linux-drivers/iio-dac/ad5764. My goal is to be able to command the DAC us…
Hello,
I've an application to use the EVAL-AD5764-4 on Linux. Since the usb interface on it only seems to work with Windows, Could one use the EVAL-ADUSB2EBZ usb to spi eval board to drive the SPI pins on the EVAL-AD5764-4?
thanks,
Scott
This DAC is a bipolar output voltage DAC.The range being +/- 10 V .If the digital data is of 16 bbits .How to feed the input along with polarity? Is it like signed 16 bit data so that 1st bit indicates the polarity of the signal?
Hi,
I am using AD5764 evaluation kit & working with evaluation software as well as STM32F407 discovery board. I have sent data from STM32 to J21 connector of AD5764 eveluation kit & woking fine.
Now I have made a PCB with reference from evaluation…
We are going for new design .Let us know ADC device compatible to AD5764 with MUX inbuilt.