• AD5761不出模拟电压

    请问,AD5761进行数模转换,可不可以直接按串行接口时序图进行配置,在SDI脚将被测数据输入,即可在Vout脚测得模拟电压,对吗?之前需不需要配置寄存器?这个是我在signalTAP里的波形图,但是在Vout脚测不到数据,在SDI、SD0处,得到的数据都与dout一样,这是为什么?(Clear脚与reset脚浮空)

  • RE: AD5761 Capacitive Load

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5761: Need DC output impedance spec for default reset state

    We need to obtain a maximum specification for the DC output impedance of the AD5761, when it remains in its default reset state after powering up. 

    The specification is needed across the full rated operating temperature of the device (all grades). 

    This…

  • procedure with ad5761

    Hello.

    I have to program an AD5716 for an output voltage from 0 to +10V.

    Is ther a sample program?
    Or where can I find sample programs?

    Best Regards.

    Renato

  • DAC IC ....AD5761  output solution

    Dear sir,

        I am also using DAC IC ... AD5761  ..using an internal reference of 2.5v ....my clock ,data ,and all signals are coming well good but I am not getting the default output voltage ....

    firstly I am not controlling it through controller ...…

  • Programming AD5761

    Hi.

    I've connected the AD5761 as from attached file.
    For the programming of the AD5761, I did the following steps:

    - write to control register 0x04 00 03 //external reference voltage (2,5V), output range =10V

    - sotware full reset 0x0f 00 00

    I load…

  • DAC ic .... AD5761 output 0V solution

    Dear sir,

        I am also using DAC IC ... AD5761  ..using an internal reference of 2.5v ....my clock ,data ,and all signals are coming well good but I am not getting the default output voltage ....

    firstly I am not controlling it through controller ...…

  • How to connect ad5761

    I would use "AD 5761" to have a 0-10V output Vout.

    I have to obtain an output voltage from 0 to +10V, having available voltages of +24V, +5v and 3,3V.

     I have only SDI, SDO, SCK and SYNC signals (as MOSI, MISO,  SCK and SS of a microcontroller…

  • how to connetc AD5761

    Hi.
    I would use "AD 5761" to have a 0-10V output Vout. I have a supply using voltage from 0V to 24V. I only SDI signals SCK and SYNC (as MOSI, SCK and SS of a microcontroller).
    I would link /LDAC to Gnd and /CLEAR to Vcc.
    This to replace a Max…

  • RE: Simultaneous reading from AD7606 and writing to the AD5671

    Sorry, the AD5761 meant everywhere in the message