• RE: AD5760评估板

    This question has been closed by the EZ team and is assumed answered.
  • AD5760 Setup Issue

    Hello!

    We are trying to get an output from the AD5760 Evaluation board which is connected to a Raspberry Pi 3 through SPI communication. I have connected the SYNC, SDIN, SDO, and SCLK pins on the board to the Pi. The Vcc is connected to 5 V on the Pi…

  • RE: AD5760 Glitch Impulse

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: An issue about AD5760

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5760 Supply Range

    The AD5760 datasheet indicates that Vdd can be as high as 30.5V with Vss being -2.5V. This falls within the listed absolute maximum ratings, however the pin descriptions and other product literature indicate that Vdd and Vss are +/- 16.5V. Would the device…

  • AD5760

    我们课题组选用贵公司 的AD5760的 评估板EVAL-SDP-CB1Z,在连线中,J3IOVCC按原理图和VCC接电源(3.3v),实际中是我们测试IOVCC和地连接的,不知道对不对,以前也在技术论坛里面发表说是不是印丝层标记错了,与原理图不符合。另外评估板的J1VCC3.3也不用外接电源都可以正常工作,求指导

  • Controlling EVAL-AD5760 board using a linux PC

    Hi-

      I would like to be able to control the voltage being put out by the DAC on an Analog Devices EVAL-AD5760_80_90SDZ board.  I have the EVAL-AD5760_80_90SDZ connected to an EVAL-SDP-CB1Z board, which in turn is connected to my linux PC via USB.  I have…

  • AD5760评估板丝印层错误

    您好:

         最近从官方购买了AD5760的评估板,在使用的过程中发现丝印层中iovcc实际上是地,接错多次 ,使用stm32驱动一直没有成功不懂硬件是否已经坏了。我看电路图,reset引脚是有上拉的,但是电压只有2.多。其他引脚入clr则有正常的3.3.(我用的电源电压是3.3)

    图片为从官方文档里面的结果 ,实物跟文档一样 iovcc 实际上是地

  • DAC芯片 AD5760调试问题咨询

    芯片:AD5760

    电源:VCC、IOVCC 3.3V;VDD12V、VSS-12V、VREFP5V、VREFN0V;

    SPI接口:SYNC、SCLK、SDIN、SDO连接单片机SPI接口;

    控制信号:LDAC拉低,CLR、RESET悬空;

    硬件电路测试,电源都对。

    软件写了个读的程序,示波器测试,没有回来的数据。

    通过读手册,时序方面看的不是很清晰!不知道能不能详细指导下,说下注意点。

    另外关于3个控制信号的使用,手册中感觉前后说的很多,很乱,搞不懂该怎么具体连接,能不能给下指导…

  • Questions on SPI of AD5760

    Hi all

    This is my first time to build a four-layer board with a such high-precision DAC. I made the system and it does not work. I do not know what is wrong.

    Could you please kindly help me to check the SPI?

    Attached files are the timing diagram captured…