• AD5754

    最近正在调试AD5754,芯片电压正常,±12,3.3v,和2.5v都正常供入。但是用FPGA写驱动程序是发现,只能读,SDO信号数据位全为0。不能够写入寄存器。下面附上我的波形

  • AD5754 - Initial write is ignored ?

    My initial write on the AD5754 is ignored ?

  • AD5754 - no output

    Hi!

    I'm using AD5754 DAC with STM32 MCU (3.3v).

    Output of DAC loaded to 5 kOhm / 200 Ohm resistor divider, Vdd is 5v, AVdd and Avss is +12 and -12 volts, reference is 2.5v. LDAC, CLR and BIN2COM are tied to 5v.

    I can program DAC (0x0c0004, 0x10000e…

  • RE: Output Variation of HMC733

    BTW, the sweeping signal is just controlled by the tuning voltage which is generated by AD5754.

  • Request for information on CONFIGURING THE AD5724/AD5734/AD5754

    Request for information on CONFIGURING THE AD5724/AD5734/AD5754

    Data Sheet AD5724/AD5734/AD5754 rev.F
    CONFIGURING THE AD5724/AD5734/AD5754:
    'The DVCC must be brought high before any of the interface lines are powered. If this is not done, the first write…

  • RE: AD5754R和STM32通过SPI通讯无输出问题

    你看AD5754的14号管脚,datasheet上是要接数字电源正,我总觉得这里是不是应该和ADuM1410的16号管脚是同一个电源正。

    AD5754输入的信号的高电位有5V。

  • hi,am interfacing with AD5754.i am not getting about clear and load command .what is the value for clear and load in control register.

    hi,am interfacing with AD5754.i am not getting about clear and load command .what is the value for clear and load in control register.

  • RE: AD5754 Exposed Paddle

    Hi,

    The substrate of the AD5754 needs to remain reverse biased with respect to all the N-wells sitting in the substrate. To do this, the substrate should be maintained at the lowest potential which is AVSS. If this is the case there will be no diodes…

  • RE: AD5754 clear issue

    Hi,

    I'm not pretty sure at the moment but most probably you can set the control register but it would not take effect until the next write. Let me confirm this in the laboratory and get back to you.

    Also, I will be moving this to the Precision …

  • RE: 这样使用AD5757和AD5754的用法是否正确

    AD5757基本正确。

    AD5754不需要在输出端链接2Kohm的电阻和4nF的电容.