• AD5753 VDPC– current draw issue

    Hi everyone,

    we designed an analogue IO module with 16 independent AIO's, divided in 8 groups of 2. Each group of 2 is supplied by an isolated DC converter providing +-20V, 42mA per rail. When testing the board we had some converters magically fail…

  • RE: AD5758 ADC Measurement of Loop Current

    Hello Maik,

    The AD5753 also had 2 external ADC inputs that can be used to monitor the control loop. There is a possibility of using the +VSENSE pin to measure the loop for the AD5758. This pin has a 50V input range so the resolution of this input is 12mV…