• AD5750 支持单电源供电吗?

    AD5750 支持12V单电源供电吗?

  • RE: Current Sinking DAC

    Regarding your question – You can certainly operate the AD5398 at a reduced current settling but unfortunately you will no longer be able to get 10 bits of resolution. It might be worth considering the AD5750 ?  This ADI IC is a current/voltage output…

  • AD5750_地引脚连接

    目前我正在利用AD5750-1做一个项目——“用于PLC和DCS应用的灵活、中级性能、电压和电流输出电路”。

    我想询问如何将AD5750接地。AD5750有两个GND引脚,引脚5靠近DVCC,引脚16靠近AVDD,我猜想引脚5是数字地,引脚16是模拟地。仅通过阅读数据手册无法确定。

    能够提供一些关于如何处理AD5750接地的建议吗?

  • Questions about chip AD5750-2BCPZ

    I am working for FPGA project using chip AD5750-2BCPZ recently,and face with some trouble:

    (1)According to the data sheet,pins( VSENSE+ and VSENSE- ) are used to protect the device, will they protect the load or just protect the chip AD5750-2BCPZ?

    (2…

  • External Rset Iout specifications

    What do the "ACCURACY (EXTERNAL RSET)" specifications mean for the current outputs of the AD5420, AD5421, AD5750 or AD5755?

  • RE: AD5750 Vsense+ and Vsense-

    Hi Mikkie,

    The +Vsense and -Vsense Pins are used for remote sensing of the load to predict and to compensate for any drops in voltage.

    If this feature is required connect the +Vsense pin to the positive side of the load and -Vsense pin to the negative…

  • AD5750 hardware mode OUTEN

    What are the OUTEN pin's levels in hardware mode, which indicate when it's
    enabled or disabled.





     

    In hardware mode, the OUTEN is enabled when the pin is high ('1') and disabled
    when OUTEN is low ('0'). Usually…
  • RE: looking for current DAC

    Hi,

    So the max output of the AD5410 product is 24mA.  The AD5410 is not a programmable voltage to current converter but a complete system solution.  If you already have a voltage that you can vary as an input one of our current drivers may be a better…

  • 类似AD5750,只需电压输出

    请问:

           是否有类似AD5750,只有电压输出的料。

    谢谢!

  • 最新ADI官方中文技术资料更新 (2015年4月)