请问4~20mA(或0~20mA)V/I芯片的输出环路顺从电压是指什么(如AD5748)?是指电流环路负载上的电压?
现在需要给1K~2K欧的电阻施加电流,电阻上的电压可能达到12V左右,AD5748是否可以?另,是否可以通过输入信号较精确的控制输出电流大小?
谢谢!
请问4~20mA(或0~20mA)V/I芯片的输出环路顺从电压是指什么(如AD5748)?是指电流环路负载上的电压?
现在需要给1K~2K欧的电阻施加电流,电阻上的电压可能达到12V左右,AD5748是否可以?另,是否可以通过输入信号较精确的控制输出电流大小?
谢谢!
Mark 3线制的4-20mA芯片,AD5420(16bit), AD5410(12bit)。
只是两者的表价均高于AD5748,TUE ±0.15% FSR vs ±0.01% FSR的缘故?
AD420和AD5420是4-20mA输出串行输入DAC,cn0270应用笔记有完整的参考电路。
http://www.analog.com/media/cn/reference-design-documentation/reference-designs/CN0270_cn.pdf
AD5748、AD5749、AD5750、AD5750-1、AD5751等都可以讲电压输入转换成4-20mA电流输出,cn0203应用笔记有AD5750-1的完整电路。
应用笔记
* AN-764:用做匹配的ADF7020 RF端口阻抗值
* AN-771:ADSP-BF533 EZ-KIT Lite与ADF70xx接口
* AN-917:配合EVAL-ADF7020和EVAL-ADF7025评估板在868 MHz和915 MHz频率下使用LC谐波滤波器
* AN-920:利用AD9788 TxDAC和ADL5372正交调制器实现单边带发射机中的增益、LO和相位补偿
*
AN-922:数字脉冲整形滤波器基础知识
* AN-0982:残余相位…
目录
What do the "ACCURACY (EXTERNAL RSET)" specifications mean for the current outputs of the AD5420, AD5421, AD5750 or AD5755?
What is the effect of my reference's variation on the output of my AD5421?
What would be the effect of the absolute accuracy and temperature drift of my external current setting resistor be to the accuracy of my AD5420's current output?