可以看一下 AD5724R AD5732R AD5734R
I am designing a UVM agent to mimic the AD5734R. I read that the internal registers are 16b and can be read out. I see the Read Timing Diagram shows SDO returns 24b of data.
What is not clear to me is the SDO data format. Does the SDO look like R, 0,…
Hi Steve,
Have you checked the Internal Reference Section of the data sheet? According to the data sheet, the on-chip voltage reference is powered down by default. If an external voltage reference source is to be used, the internal reference must remain…
I am using AD5752R in 0-10V operation. But its getting configured only to 0-5V range. Wat may be the reason?
If SYNC pin is high Is the SDO pin of the AD5722R tri stated ?
Can several AD5722R devices share one common SDO line on the data bus and just be selected by the SYNC input?
Or will each of them need its own SDO line or be daisy chained?
In the AD5752 datasheet a power up time of 10uS is required before writing to the DAC - what happens if I write to the DAC before this?
My initial write on the AD5754 is ignored ?