• RE: AD5696 Vref power up behaviour

    Hi ,

    Are you indeed using the AD5696 and not the AD5696R? 

    Have you tried setting /RESET pin as logic high before supplying and enabling the external reference and see what happens?

     

    Cheers,

    Ivan

  • RE: EVAL-AD5689RSDZ user guide and evaluation software

    你好,依據EVAL-AD5686R user guide描述,軟件是使用ACE.

    我安裝了ACE及AD5686R的ACE pulgin.

    在ACE界面可以看到AD5689R EVK,雙擊後出現沒有plugin.

    請問是哪裡出問題呢?

    另外也試過AD5686R EVK軟體.

    該軟體並沒有看到AD5689R的選項.

    不管是選AD5686R或是AD5696R的選項後,都沒有認到AD5689R的EVK.

    請問是哪裡操作錯誤呢?

    謝謝.

  • nanoDAC+ family

    SPI INTERFACE

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI nanoDAC+, with ±2 (16-Bit) LSB INL

  • AD5691 driver support ?

    Hello,

    Anlog wiki contains drivers for AD569x family, but AD5691 is not listed in the wiki's list:

    AD5696R - Microcontroller No-OS Driver [Analog Devices Wiki] 

    Is AD5691 supported with the generic AD569x driver ?

    Thanks,

    ranran

  • RE: How do I use ACE software to transfer digital quantity to analog quantity continuously in AD5696

    Hi,

    Unfortunately the functionalities of the evaluation software is limited. But you can use a microcontroller with the AD5696R no OS driver and connect it to the PMOD connector of the evaluation board.

    Cheers,

    Ivan

  • Could you give me the Labview source for AD5696 and SDP-S

    I bought the AD5696 evaluation board  EVAL-AD5686RSDZ and control board EVAL-SDP-CS1Z,I can use AD5696R evaluation software to convert a digital quantity into analog quantity manually, but I need to convert digital quantity into analog quantity continuously…

  • RE: AD5698R READ OPERATION

    Hi,

    I couldn't understand.

    Sorry it was my typo. The device is AD5696R.

    As for Figure51 in the AD5696R datasheet, START BY MASTER --> ACK. BY MASTER --> ACK. BY MASTER.

    and REPEATED START BY MASTER --> ACK. BY MASTER --> ACK. BY M…

  • RE: What is nanoDAC+?

    Single, Dual and Octal versions have been added to the nanoDAC+ family...

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI…

  • nanoDAC+ Family AD531x/AD568x/AD569x/AD567x

    Q1. What is new?

    A1. The nanoDAC+(TM) family offers improved analog performance in terms of INL and glitch energy specifications.. Some members of the family, those with a part number ending in 'R', for example AD5686R, include a  low drift 2.5V…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…