• AD5693 I2C pin fall time requirement

    Hi.

    We are using DA-converter AD5694 in out design.

    I2C bus speed is close to 400kHz i.e it is used in fast mode. I2C specification state the same requirement for signal fall time as is stated in AD5694 data (table 4, page 4)

    Requirement for the fall…

  • nanoDAC+ family

    SPI INTERFACE

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI nanoDAC+, with ±2 (16-Bit) LSB INL

  • RE: AD5698R READ OPERATION

    Hi,

    I believe this is a typo error as there is no AD5698 part. I think you are referring to either AD5696 or AD5694 which are almost identical when it comes to the digital communication.

    When writing to the part, the microcontroller acts as the master…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • nanoDAC+ Family AD531x/AD568x/AD569x/AD567x

    Q1. What is new?

    A1. The nanoDAC+(TM) family offers improved analog performance in terms of INL and glitch energy specifications.. Some members of the family, those with a part number ending in 'R', for example AD5686R, include a  low drift 2.5V…