Can I connect 2.7V to VDD and 3.3V to VLOGIC? In general, can VLOGIC be higher than VDD?
Hi,
I want to add AD5693 nanoDAC converter into one of my upcoming product. I am not able to find a matching Linux device driver for the AD5693 converter at Linux Drivers [Analog Devices Wiki]
1) Please let me know where I can get the reference Linux…
Hi.
We are using DA-converter AD5694 in out design.
I2C bus speed is close to 400kHz i.e it is used in fast mode. I2C specification state the same requirement for signal fall time as is stated in AD5694 data (table 4, page 4)
Requirement for the fall…
Dear All,
Is it possible to Vout pin = 0~10V for AD5693 when Vref=5V, VDD=5V,Vlogic=3.3V?
Best regards,
Evan
大家好,我想用AD5683、AD5693输出0至10V的信号。
当AD5683、AD5693内部增益为2(配置输出为2xVref),Vref=5V,VDD=5V,Vlogic=3.3V时,能够输出0至10V的模拟信号么?
谢谢!
Single, Dual and Octal versions have been added to the nanoDAC+ family...
AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference
AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference
AD5683: Tiny 16-Bit SPI…
SPI INTERFACE
AD5683: Tiny 16-Bit SPI nanoDAC+, with ±2 (16-Bit) LSB INL
中文数据手册
AD845 精密、16 MHz、CBFET运算放大器
AD5693R/AD5692R/AD5691R/AD5693小型、16/14/12位I2CDAC+,具有±2LSBINL(16位)和2ppm/°C基准电压源
AD8220 具有轨到轨输出的JFET输入仪表放大器,采用MSOP封装
AD8613/AD8617/AD8619 低成本、微功耗、低噪声、CMOS轨到轨输入/输出运算放大器
AD9656 四通道、16位、125 MSPS JESD204B 1.8 V模数转换器…