• RE: EVAL-AD5689RSDZ user guide and evaluation software

    你好,依據EVAL-AD5686R user guide描述,軟件是使用ACE.

    我安裝了ACE及AD5686R的ACE pulgin.

    在ACE界面可以看到AD5689R EVK,雙擊後出現沒有plugin.

    請問是哪裡出問題呢?

    另外也試過AD5686R EVK軟體.

    該軟體並沒有看到AD5689R的選項.

    不管是選AD5686R或是AD5696R的選項後,都沒有認到AD5689R的EVK.

    請問是哪裡操作錯誤呢?

    謝謝.

  • AD5685R external reference

    Hello

    Can AD5685R use 4.096V or 2.048V external reference ?

    My customer would like to use AD5686R for 14bit, 4ch and  small package at 4.096V full-scale.

    The datasheet says that  impedance of REF pin is very low and  the internal reference 2.5V is enabled…

  • RE: AD5681R long-term Drift

    Hi ,

    Unfortunately, that's all we have, you may use the same data as AD5686R's.

    Cheers,

    Ivan

  • RE: AD5320 spice

    Hi,


    Just in case you will be needing four channels with unipolar outputs, you might want to consider AD5686R which has a SPICE model available.

    https://www.analog.com/en/products/ad5686r.html#product-overview

    Cheers,

    Ivan

  • AD5686 Vlogic level and GAIN pin

    Hello,

    I am looking at the datasheet of the AD5686/AD5684 (revision C) and there are two somewhat unclear topics I was hoping someone could help me with.

    1. Vlogic level in relation to Vdd:

    On page 6, note 1 says that the SPI speed of 50MHz is only valid…

  • 可编程电源芯片

    我现在需要一个可编程·电源芯片,要求输出在0到5V之间可调,输出电流在大概需要120mA,请问有没有类似AD5686R的芯片介绍

  • nanoDAC+ family

    SPI INTERFACE

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI nanoDAC+, with ±2 (16-Bit) LSB INL

  • supply voltage vs. output/input voltage on DACs and ADCs

    Hello,

    I am interested in using AD5686R and AD7682 for a lightweight analog data acquisition system. Right now, I am thinking about how to properly power these devices. One of my design constraints is that the device must be powered by a wall wart with…

  • RE: AD5683R internal Reference long term stability

    Hi,

    You may use AD5686R's long term temperature drift (figure 58, page 27) as a reference, but please do note that we cannot guarantee the same performance as the two devices are not exactly the same. 

    Cheers,

    Ivan

  • 视频介绍:用于I/O卡和PLC应用的4通道、灵活、可配置、电压和电流输出电路 (CN0229)

    视频介绍:用于I/O卡和PLC应用的4通道、灵活、可配置、电压和电流输出电路 (CN0229) by adiadmin

    该电路是一种仅使用两个模拟器件的多通道、灵活的模拟输出解决方案,它满足多通道I/O卡、可编程逻辑控制器(PLC)和分布式控制系统(DCS)应用的大部分要求。具有轨到轨缓冲输出的四通道、16nanoDAC+ AD5686R 配合四个工业电流/电压输出驱动器 AD5750-2 使用,可提供所有典型的电流和电压范围的输出,其具有16位分辨率且无失码、0.05%的线性度以及小于0.1…