• RE: AD5682R Power -On Reset

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Can the AD5310R "SHORT WRITE OPERATION"?

    Hi

    My customer is considering AD5310R.


    The AD5310R data sheet says “If SYNC is high after 16 falling clock edges occur, it is interpreted as a valid write and the first 16 bits are loaded to the input shift register.”
    However, SPI Command Operation…

  • nanoDAC+ family

    SPI INTERFACE

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI nanoDAC+, with ±2 (16-Bit) LSB INL

  • RE: high voltage current sink&source DAC

    Thanks for the hint with the AD5683R/AD5682R/AD5681R/AD5683, which are interestingly smaller than the AD5621 although both are LFCSP and the former has 8 instead of 6 pin (normally I would expect that same package type and more pins would mean bigger…

  • RE: What is nanoDAC+?

    Single, Dual and Octal versions have been added to the nanoDAC+ family...

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • nanoDAC+ Family AD531x/AD568x/AD569x/AD567x

    Q1. What is new?

    A1. The nanoDAC+(TM) family offers improved analog performance in terms of INL and glitch energy specifications.. Some members of the family, those with a part number ending in 'R', for example AD5686R, include a  low drift 2.5V…