• AD5681R Thermal Hysteresis

    Hi

    My customers are considering the AD5681R.
    I got a question about temperature hysteresis there.

    I think that the temperature hysteresis is evaluating the characteristics by switching the temperature in order of ambient temperature, -40 ° C, 105 ° C,…

  • AD5681R long-term Drift

    Hi,

    My customers are considering the AD5681R.
    So I got a question.

    Is there data on long-term stability of AD5681R?
    Especially, I want error data of the initial (about 100 hours) after turning on the power supply.

    I found the answer below but I'm happy…

  • AD

    Hi all,

    In my project AD5681R is chosen to provide analog output signal under 3.3 (V) operation condition (or 5V operation condition)

    According to datasheet, following descriptions are given

    1-) AD5681R has two types of referances which are called internal…

  • Can the AD5310R "SHORT WRITE OPERATION"?

    Hi

    My customer is considering AD5310R.


    The AD5310R data sheet says “If SYNC is high after 16 falling clock edges occur, it is interpreted as a valid write and the first 16 bits are loaded to the input shift register.”
    However, SPI Command Operation…

  • nanoDAC+ family

    SPI INTERFACE

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI nanoDAC+, with ±2 (16-Bit) LSB INL

  • RE: dac选型求助

    您可以参考一下AD5691R 或者 AD5681R

  • RE: high voltage current sink&source DAC

    Thanks for the hint with the AD5683R/AD5682R/AD5681R/AD5683, which are interestingly smaller than the AD5621 although both are LFCSP and the former has 8 instead of 6 pin (normally I would expect that same package type and more pins would mean bigger…

  • RE: What is nanoDAC+?

    Single, Dual and Octal versions have been added to the nanoDAC+ family...

    AD5681R: Tiny 12-Bit SPI nanoDAC+, with ±1 LSB INL and 2 ppm/°C Reference

    AD5682R: Tiny 14-Bit SPI nanoDAC+, with ±2 LSB INL and 2 ppm/°C Reference

    AD5683: Tiny 16-Bit SPI…

  • AD5682R Power -On Reset

    Hello All,

     

    I have some questions for AD5682R Power-On Reset.

    Looks like datasheet does not state the details…

     

    Q1) What is the threshold voltage value for POR?

    And which pin’s voltage level does monitor for? VDD and or VLOGIC?

    (Please see the…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…