• RE: Request recommended Voltage out DAC solution supporting +- 25V output range

    Hi Se-woong, 

    You can do:

    1) AD5535B (0-50V 32Ch) + offset amplifier (8* ADA4522-4 is a good choice) 
    -Something seems wrong with the website and I can't paste images.
    Additional >50V supply needed for the AD5535B.

    2) 2*AD5679R (0-2.5V/5V 16ch) + Offset…

  • A Fantastic Voyage

    One of my favorite movies growing up was the science fiction film “Fantastic Voyage,” in which a submarine with a team of scientists are shrunk to molecular size and injected into a man in order to find and destroy a life-threatening brain tumor. In the…

  • FAQ: How to control ADI DAC Evaluation Boards (EVB) using python scripts?

    Most of the latest ADI DAC EVBs are controlled by the ACE software. By making use of the ACE Remote Control function, DAC EVBs can be controlled via a python script.  

    There are two practical ways to create a python code to remotely control the ACE software…

  • 2020年 ADI 20款硬核新品,为你献上电路设计的不二之选

    你最关注的领域是什么?ADC/DAC?Power?RF?.....

    你知道ADI在这些领域都推出了怎样的硬核新品吗?

    回首2020年,虽然被疫情干扰,不过咱ADI依旧没有停止推出新产品的脚步,今天斑竹就为大家盘点一下今年的“新秀”吧~

    四通道、软件可配置输入/输出 AD74412R/13R

    AD74412R 是一款适用于楼宇和过程控制应用的四通道软件可配置输入/输出解决方案。AD74412R 包含用于模拟输出、模拟输入、数字输入和电阻温度检测器 (RTD) 测量的功能,这些功能集成在一个单芯片解决方案中…