• RE: AD5678 and AD7193: Problem while using simultaneously.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 求助ad5678?

    AD5678 利用SPI输出一个特定的电流,之后,再用SPI输出一个相同的电流,中间会有跳动或抖动吗?

    ps: 我是想利用AD5678 输出一个恒定电流,可能是板子设计不好,受外界干扰电流会变化,所以想间隔一段时间重新设定相同电流,但是不知两次设置电流时中间会不会有变化,或抖动?

  • 求助AD5678的问题

    AD5678 利用SPI输出一个特定的电流,之后,再用SPI输出一个相同的电流,中间会有跳动或抖动吗? ps: 我是想利用AD5678 输出一个恒定电流,可能是板子设计不好,易受外界干扰,电流会变化,所以想间隔一段时间重新设定相同电流,但是知两次设置中间电流是否会有变化?

  • RE: Request suggestions for Drop in Replacements for AD5668

    AD5678 is pin compatible in TSSOP-14 and TSSOP-16. AD5676 is functionally equivalent but not pin compatible.

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…

  • nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…