• nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • Couple of questions re: AD5629R power-down behavior

    Hi -- I've got two questions on the data sheet for the AD5629R (Rev. D).

    1) Page 21 says that "Individual channel power-down is not supported while using the internal reference."  Does this mean that none of the 0100 commands (Power down…

  • ADI公司解决方案通报—数模转换器IC

    目录


    • 提供动态功率控制的DAC
    • 低功耗DAC可节省功率
    • 突破性1 ppm DAC
    • 基站发射架构中的IF DAC解决方案
    • 新款DDS IC功耗更低、尺寸更小
    • 多路输出低抖动时钟发生器
    • 数据转换知识资源
    • 低功耗精密运算放大器用作DAC缓冲器
    • 选型指南
    • RF DAC实现单封装比特流到射频转换解决方案
    • 用于无线通信设备的混合信号前端IC
    • 采用WLCSP封装的8通道denseDACRegistered .
    • 采用紧凑型封装的多功能、易用、精密DAC
    • 新型系…
  • AD566x/4x/2x(R) -  Supply Voltages & On-chip Reference options

    The AD5664R has two on-chip reference options available, 1.25V and 2.5V. What is the recommended supply voltage in each case?