• AD5667 on Pi - Analog Output checking

    Hello,

    I'm trying to generate a sinewave utilizing a I2CDAC >>> AD5667 that is caped on a Raspberry Pi. 

    I'm struggling with checking whether or not the chip/device is being talked to from the Pi. 

    I'm using this library to generate voltage…

  • RE: AD5667 I2C interface  C code example

    // Distributed with a free-will license.
    // Use it any way you want, profit or free, provided it fits in the licenses of its associated works.
    // AD5667
    // This code is designed to work with the AD5667_I2CDAC I2C Mini Module available from ControlEverything…

  • RE: I2C Read - AD5667

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Send Analog pulse to the motor drive using AD5669 I2C module

    Hi, I have been working on an automatic parking system and to control the motor drive Barrier I want to send an analog signal to the motor driver to switch on the barrier but being new to this I am using AD5667 I2C module.

    I need some suggestion to make…

  • AD5696R multiple write

    Hello. Could AD5696R work in multiple write mode like AD5667 ?

    Our customer connect  AD5667  to slave address and send some blocks  (each 24bit - command+data) and then STOP.

    SLAVE ADDRESS - (comand+data)-(comand+data)-(comand+data)-........(comand+data…

  • AD5667R I2C无应答

    设计中采用了AD5667R,但是在使用DSP对其进行控制的时候AD5667一直没有产生ACK。请问读写AD5667R有其他顺序要求吗?注:从机地址设置的是0x1E.(adr接地)

  • RE: API/SDK for AD5667REBZ

    Hi Mark,

    Thanks.

    My customer bought Galvo system. The Galvo System includes AD5667REBZ evaluation board of Analog Devices. This board allows manage galvanometers. The CD with test application is attached to the evaluation board. But they would like…

  • AD7785 Eval Board connect with C# or VB

    It seems the code here could be modified to connect to the AD7785 Eval Board:

    ftp://ftp.analog.com/pub/evalcd/AD5667/code%2064%20bits/USBStuff.bas

    ... but what is the PID for this board? (I assume the VID is the Vendor ID which is still 1110.)

    Thanks…

  • API for AD5667REBZ

    Hello,

    My name is Meir and I am DFAE from Phoenix Technologies in Israel.

    Ability, one of my customers, bought evaluation board : AD5667REBZ.

    This board allows manage galvanometers. The CD with test application is attached to the evaluation board.

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…