• RE: About EVAL-AD5665R win8.1 64bit USB-DRIVER

    Hi Keiichi,

    I'm sorry but the board you are referring is obsolete, and we do not provide support anymore.

    Being said that, lets check if this solution works,

    Install the Drivers.exe first. Once it is installed, copy the AD5665.exe into PROGRAMFILES…

  • RE: AD5665R配置不正常

    依据现象判断,很可能是负载电流过大导致DAC器件无法正确响应(几十毫安电流对DAC是很大的)。AD5665供电流和吸电流的能力可以参考数据手册中的图40和图41. 建议调整负载降低所需的电流。

  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…

  • nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…