• AD5660: Can multiple AD5660 devices be updated simultaneously?

    Can multiple AD5660 devices be updated simultaneously?

     

    No, this is not possible with AD5660, You should use AD5542 or AD5570 as these
    devices have /LDAC pin to achieve this.

  • RE: 关于AD5660参考电压

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5660

    Hi,
    Can I use the AD5660 -3 digital to analog converter with 2.5v reference voltage, and 3.3v VDD voltage, to get a VOUT range of 0 to 3v?
    (The datasheet only presents 2 design options: 1.25v REF voltage with 3.3v VDD, and a 2.5V REF voltage with 5v VDD…

  • RE: AD5660 with Internal ref 1.25V 5ppm : Refout=2.5V 400ppm ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5660 通过FPGA SPI控制,器件无响应

    通过FPGA产生SPI控制信号控制AD5660, 在片选信号为低不管是采用连续时钟还是门控时钟,芯片均无输出响应 ,试验过 10M时钟 ,6M时钟 ,4M时钟 ,片选内为低期间保持24个时钟或者27个 时钟都无响应 ,不知道哪里出问题了

  • RE: EVAL-AD5660: Source code of the included GUI and firmware

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • 有没有精度高、温漂低、与AD5660引脚相同的DAC?

    我们在开发一个产品时,要求产生直流电压0-2.5V,精度要求高。以前用的16位AD5660,发现误差有些大,有时达到5mV,有没有误差极小、温漂更小的能代替AD5660的DAC推荐?引脚如果相同更好?

  • EVAL-AD5662/AD5660/AD5640/AD5620

    Hi everyone!

    I'm using EVAL-AD5662/AD5660/AD5640/AD5620 and have AD5660 as my DAC and I noticed that there are grounding problems to the AGND and DGND pins of the evaluation board. It is said in the datasheet of the evaluation board that the analog GND…

  • DA转换器中数据转换问题

    最近在使用AD5660芯片,有个不明白的问题想请教。在数据手册中,Vout=2*Vrefout*D/65536,在此选用的Vrefout为2.5V,现在想问的是,如果想输出0.895V的电压值,那么根据公式D=Vout*65536/2/Vrefout,这样得到的数据D就不一定是十六位的整数。D值就无法按十六位数据格式通过微处理器发送到AD5660中,实现所需的输出。请高手帮忙