• AD5643R-5 cannot output voltage

    I tied /LADC pin to GND, and /CLR pin to VDD on hardware connection.

    I used an FPGA  to sent config signals to AD5643.

    First I sent 00_111_000_0000_0000_0000_0001 to use the internal reference, I can see a 2.5V output on the  REFOUT pin.

    Then I sent 00_011_111_1111_1111_1111_1111…

  • RE: AD5643R full scale output range

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…

  • nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…

  • AD566x/4x/2x(R) -  Supply Voltages & On-chip Reference options

    The AD5664R has two on-chip reference options available, 1.25V and 2.5V. What is the recommended supply voltage in each case?

  • ADI芯片辨识、型号查找

    看看截图:

  • 【ADI实验室电路合集】第2册PDF下载

    如题,灰常实用的资料。

    第一册在这里下载:【ADI实验室电路合集】第1册PDF下载:http://ezchina.analog.com/thread/6847

  • 分享ADI中文参考电路好资料,欢迎下载交流_01

    分享ADI中文参考电路好资料,欢迎下载交流_01