• AD5641 sink and source capability (ΔVout vs I)

    Hello,

    Is there a typo on Figure 21 in AD5641 datasheet? What is a scale for ΔVout? V or mV?

    Regards,
    Ivan

  • RE: AD5641 ouput voltage quandary

    Hi,

    I resolved this issue a while ago and to be honest I cannot remember what the solution was. But thank you for your response.

    Richard.

  • RE: AD5641 evaluation

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: IBIS model for AD5160 and AD5641

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD5641 generating glitches in a sine wave with DC offset

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5641: What's the expected behavior when shorting DAC output to ground?

    What can I expect if the AD5641 output is shorted to ground?

    The datasheet shows a short circuit current of 15mA but no other references to this type of fault. 

  • AD5641 SPI communication with Arduino

    Hey everyone I have a problem communicating with a AD5641 DAC. I am making this project with Arduino UNO and I can't seem to figure out how to properly send data to the DAC. If someone can give me an example or explain how to send data to this DAC I'd…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…

  • nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…