• AD5640: Increasing gain

    If I want an output from 0V to 3.3V (in a system with a 3.3V supply) can I put
    a resistor between the output pin and the FB pin to increase the gain from 2 to
    2.6?

     

    This is not the best approach.  The device is internally trimmed to comply with…

  • RE: AD5620 or AD5640- Using Vfb to control the DAC output

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • EVAL-AD5662/AD5660/AD5640/AD5620

    Hi everyone!

    I'm using EVAL-AD5662/AD5660/AD5640/AD5620 and have AD5660 as my DAC and I noticed that there are grounding problems to the AGND and DGND pins of the evaluation board. It is said in the datasheet of the evaluation board that the analog GND…

  • 使用寿命

    AD5640BRJZ的使用寿命/年限是多少?

  • RE: looking for reference circuit of AD9834 to op amp

    Hi Miguel,

    The specifics of some of the parameters are still to be determined but the supply voltage and output range would be about 20V, max current output could be about 100ma, Not sure about the impedance.  It would need high amplitude resolution so…

  • AD5620 Model Options

    i have a question about AD5620 Model Options.

    what difference between AD5620A..., AD5620B... and AD5620C...? Difference is only in relative accuracy between models (A the best?)

    next, AD5620-2-3 parts include an internal, 2.5 V, 5 ppm/°C reference,…

  • EVAL-AD5660: Source code of the included GUI and firmware

    Hi all,

    I am currently evaluating EVAL-AD5660 and i am getting erroneous output in the GUI reading of the voltage. At full scale, I am getting a 2.75V reading but the device should only have a 2.5V full scale reading. (Vref = 1.249V).

    I have checked…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…