• AD5628 OFFSET

    I'm using the DAC AD5628 for an automotive application. Reading the component

    datasheet I did not understand how much the offset error is. By considering the
    datasheet at page 14 , figure 26 and 28 seems to have a discrepancy : the
    offset at 25…

  • AD5628 IBIS MODEL

    Hi

    Can we use IBIS AD5648 IBIS MODEL  for AD5628?

    (or Can we download AD5628 IBIS MODEL)

    Best Regards

    Thank you very much  

  • AD5628 WITH LABVIEW

    Hello,

    I am trying to set the Internal Reference Register by using labview functions but I was unable to do because of uncertain on frame format.Can you please suggest me a frame in array format to set

    Internal Reference Register ON.

    I have used many…

  • AD5628 No Device Handle

    Hi all,

    I am using ad5628 DAC with RaspberryPi 3 Board , I have found drivers for ad5604 (Linux/drivers/iio/dac/ad5064.c - Linux Cross Reference - Free Electrons ) , I belive that it will work for ad5628 also . 

    I have enabled the ad5604 in the linux…

  • AD5628 : characteristic of output noise

    Hi,

    The output noise of AD5628 is 12 uVp-p in Table3 of the data sheet.

    However, the plot of Figure 45, 46 and 47 shows a big output noise.

    Is this graph correct?

    If the graph is wrong, I want to see a correct graph.

    Best Regards,

    Mr.K

  • AD5628 reset DAC to zero problem

    I use AD5628ACPZ-2-RL7 DAC in my device and I can't make it works stable. Some times all DACs go down. I do not know reason why.

    - I use 0.1 uF and 10uF between Reference and GND.

    - 22uF tantal and 0.1uF between Power to GND.

    - CLR pin is on the…

  • RE: using AD5628 with Arduino Uno

    Hi Mike,

    On the wiki you can find an example of interfacing the AD5628: http://wiki.analog.com/resources/tools-software/uc-drivers/microchip/ad5628

    Let us know if it's not helpful for you.

    Thanks,

    Dragos

  • AD5628-2 Characteristics (Output range and -X)

    Hi

    We will use 2.5V or 5V output DAC.(8ch)

    These Outputs connect to some amp. 

    AD5628 specifications have two VDD condition.(VDD=4.5V to 5.5V and  2.7V to 3.6V) 

    Can we find AD5628-2 2.5V outputs with external VREF=2.5V?

    (Can we get below character with…

  • Question on AD5628 Vref in/out

    Hi,

     

    The AD5628BCPZ datasheet is a bit confusing.

     

    There is only one pin (#6) nammed Vrefin/Vrefout. The datasheet (page 21) states that when the internal reference is on, its voltage is available at pin #6 (cause an decoupling cap is advised). And…

  • Where do I tie the exposed paddle on DACs such as the AD5541A, AD5542A, AD5512A, AD5668, AD5628, AD5669 and AD5629 that are packaged in LFCSP?

    Where do I tie the exposed paddle on DACs such as the AD5541A, AD5542A, AD5512A, AD5668, AD5628, AD5669 and AD5629 that are packaged in LFCSP?