• Output voltage problem.(AD5625R)

    Hi,
    I want to control the output with I2C.
    The pin settings are as follows:
    LDAC = Low, CLR = High, POR = Low, VDD = 5V
    After writing 0x01 to the 0x38(internal reference on) register, Ref Voltage(2.5V) is output.
    However, 4V is output from VoutA,B,C,D.(Gradually…

  • How to AD5625R Output voltage setting?

    Hi,

    I want to control the output with I2C.

    The pin settings are as follows:

    LDAC = Low, CLR = High, POR = Low, VDD = 5V

    After writing 0x01 to the 0x38(internal reference on) register, Ref Voltage(2.5V) is output.

    However, 4V is output from VoutA,B,C,D…

  • AD5625R I2C INTERFACE CODE FOR 8051 MICROCONTROLLER

    I am using AD5625R for generating reference voltages. But I am unable to generate the voltages. I thick there is some probl. with I2C Coding using 8051 microcontroller. I need the code to generate the voltages

  • AD5625R I2C: We can't it to output any voltage


    Hi

    We have been trying to get the AD5625R DAC (with I2C) to work, we have spent more than a week trying to implement the datasheet instructions, but with no success. Can you give us some hands on this please.

    Thanks,
    Yaqoob

  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…

  • nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD566x/4x/2x(R) -  Supply Voltages & On-chip Reference options

    The AD5664R has two on-chip reference options available, 1.25V and 2.5V. What is the recommended supply voltage in each case?