• AD5624R output is not coming on any channels.

    Hi 

    First of all I have given the soft reset command and waited for 1ms. I gave the power up command for all the channels of DAC and  followed the internal reference off command to DAC.Then written the 0x18FFF0 to configure the DAC-A for full scale ouput…

  • RE: AD5624R output shutoff

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Are there non-reference options available of the AD5664R and the AD5624R?

    This question has been closed by the EZ team and is assumed answered.
  • AD5664 Linux Driver for Python

    Hi guys, 

    I have a customer who wants to control AD5664 using raspberry pi, he is coding in python. I found we have the Linux driver below. Do we have one for python or can we use the existing one?

    https://wiki.analog.com/resources/tools-software/linux…

  • Connecting the SPI signals to 3.3v Master when AD5624RBCPZ-5R2 powered by 5v

    Hi,

    We are using AD5624RBCPZ-5R2 in our design.

    We have connected the VDD(Pin 9) pin to 5v.

    Now we want to control AD5624RBCPZ-5R2 using SPI signals which is connected to FPGA bank which is powered by 3.3v.

    Will there be any problem in our approach?

    An…

  • RE: Question about AD5724 Power Control Register

    Hi ,

    Just want to be sure, are you using AD5724? Or is it AD5724R? 

    AD5624R's Power Control Register [DB4] is assigned as PUref, which has a default value of 0 which means the internal reference is in power-down mode, it needs to be set to 1 to power…

  • RE: Exposed Pad in AD5664/AD5624

    The paddle should be connected to GND. This will also apply to the AD5624R/AD5644R/AD5664R

  • RE: AD5752 SPORT usage

    Hi Sebastian,

    Unfortunately, I could not find any code example for /SYNC synchronisation.

    The following link refers to the ADSP-BF59X Blackfin Processor in which file there are some programming examples for the SPORT Controller.

    http://www.analog.com…

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…